Poor Graphics performance with android kk4.4.2/rel_imx_3.10.17_1.0.0_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Poor Graphics performance with android kk4.4.2/rel_imx_3.10.17_1.0.0_ga

1,495 Views
oussama
Contributor III

I'm having poor graphics performance with android kk 4.4.2 /  rel_imx_3.10.17_1.0.0_ga on imx6q board. I only see the issue when using LVDS display, I do not see the issue when I use HDMI display.

As a result the mouse cursor is not redrawn smoothly when I move the mouse.

The fps of hdmi is about the double of lvds when benchmarking it.

- why do I see the issue only on lvds?

- Do I need to update my opengl libs? currently I'm using default one provided by 442

0 Kudos
Reply
4 Replies

1,231 Views
oussama
Contributor III

The yocto project provide gpu-viv-bin-mx6q-3.10.17-1.0.0-hfp.bin for regular linux rootfs. Does freescale provide gpu viv libraries for android compatible with 3.10.17?

0 Kudos
Reply

1,231 Views
SergioSolis
NXP Employee
NXP Employee

No, they are compatible with 3.0.35 and Vivante v4.6

KK4.4.3 are compatible with 3.10.17 and Vivante v5

0 Kudos
Reply

1,231 Views
SergioSolis
NXP Employee
NXP Employee

Hello Oussama,


Have you tried using the newest bsp available KK4.4.3.2 ?, it has a newer GPU library.

I would recommend that you migrate to the newer bsp.

0 Kudos
Reply

1,231 Views
oussama
Contributor III

Hello Sergio

Unfortunately, I need to use kk 442/3.10.17.

Oussama

0 Kudos
Reply