Plug usb 3.0 camera into imx8mq get error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Plug usb 3.0 camera into imx8mq get error

2,666 次查看
charleshuang
Senior Contributor II

Hi
BSP : Yocto 4.14.98_2.0.0

I plug an usb 3.0 camera into imx8mqevk board , it will get error as below

[  204.132368] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[  205.808374] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

Could you tell me how to fix this issue?

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,565 次查看
charleshuang
Senior Contributor II

Hi

But we have already test different cable as below

USB 3.0 cable(3m/50cm) , it's fail

Then we insert USB 3.0 HDD, it's okay

And we test the camera on i.MX 8X , it's work well

Are there any other suggestions?

thanks

0 项奖励
回复

2,565 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Charles,

I have verified USB 3.0 device connecting to USB 3.0 port on MX8M, there is no problem, it worked normally.

 

Probably there is problem with USB cable, we have several USB cables, some can work, but some cannot. and that error appears.

Regards

0 项奖励
回复

1,938 次查看
solve_this
Contributor II
 
0 项奖励
回复

1,935 次查看
solve_this
Contributor II

Did you solve this one brother

0 项奖励
回复