Plug & Trust MW SD Card Image SE050+IMX6UL source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Plug & Trust MW SD Card Image SE050+IMX6UL source code

1,666 Views
wangxuehua
Contributor I

Hello, Could you tell me where can I get the source code of imx-4.14.98-2.0.0-02.12.00.img which is download from https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-trust-se...  —— Tools and Software——Plug & Trust MW SD Card Image?

Tags (1)
0 Kudos
Reply
1 Reply

1,660 Views
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

The source code of the kernel can be get from the BSP build. We use Yocto to build the BSP.

You can get the documentation from here.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Then follow the i.MX_Yocto_Project_User's_Guide.pdf to build the BSP. After built successfully, the source code can be found in the <yocto_folder>/<build_folder>/tmp/work/<board_folder>/linux-imx

 

And here is the web page version for the kernel source code

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga

0 Kudos
Reply