Please help me to suggest a part number for the below spec.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Please help me to suggest a part number for the below spec.

741 次查看
daviddunn
Contributor I

-NXP iMX7
-Dual ARM Core A8+, 1Ghz+
-2 X 10/100 Eth Controllers MAC
-UARTS (5+)
-CAN( 1)
-SPI _ HS > 40Mhz (3), I2C(2)
-USB OTG/HS (1)
-OS: Linux
-Target cost  b/w  $10-$15 / 1K
-WiFi /BLE (Optional)

0 项奖励
回复
1 回复

680 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Sorry, we do not have devices with Dual ARM Core A8.

Nevertheless, I think the mentioned i.MX7(D) is one of suitable candidates,

but its SPI is not so speedy as requested in Your parameters.

 

i.MX 7Dual Arm Cortex-A7 Processor|NXP 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复