Pin status for iMX8M plus soc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin status for iMX8M plus soc

894件の閲覧回数
KalpeshD
Contributor I

Hi Team NXP,

Refer below snapshot of the datasheet.
Highlighted pin status as mentioned. Is this "RESET CONDITION" mean to the status of pins while the SOC is in reset condition(J29 pin_POR is low) or soc reset release condition(J29 pin_POR is high) ??

If this is of during reset condition then what could be the pin status after reset release and till before we configure IO pins to required levels?

KalpeshD_0-1732714773288.png

Waiting for the clarification for this topic. Thanks. 

 

 

0 件の賞賛
返信
1 返信

866件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

The RESET CONDITION is after POR_B rises.

During reset condition, we couldn't manage the GPIOs nor the status of them. The reset condition assigns a default function to every pin after POR_B rises, so BootROM is executed correctly and the boot pins are ready to be sampled.

This condition means that boot modules are initialized at BootROM level, GPIO wouldn't but USDHC, NAND, FlexSPI, USB, etc.

Regards

0 件の賞賛
返信