Pin mux tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin mux tool

10,869 Views
MadhuriAkkenepa
Contributor II

What are the differences between the interactive i.MX pin mux tool vs the PINS-TOOL_IMX?

Is the PINS-Tool-IMX the recommended too for pin configuration?

Search Results: iomux tool imx6 

Pins Tool for i.MX Application Processors|NXP 

4 Replies

7,750 Views
gusarambula
NXP TechSupport
NXP TechSupport

Yes, the latest revision of the Pins Tool (v4.0) does have support for the i.MX6 SCM parts (Dual, Quad and SoloX).

0 Kudos
Reply

7,750 Views
scottfowler
Contributor IV

I have the same question, does the pin mux tool support the i.MX6 SCM's?

0 Kudos
Reply

7,750 Views
timlapsley
Contributor I

Hi Gursarmbula,

Does the latest version support SCM-IMX6 processors as well? In particular SCM SoloX ?

0 Kudos
Reply

7,750 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Madhuri Akkenepalli,

The latest tool available, which I would recommend using if you haven’t started with another tool is the Pins Tool for i.MX Application Processors V2.0. This tool is available on the link below under Software:

http://www.nxp.com/products/software-and-tools/software-development-tools/processor-expert-and-embed...

There are Linux and Windows version and online and offline installers. This tool allows you to set the Pin Mux options in an intuitive GUI and also generates code to configure these options on the BSP. There is more information on how to install it on the following document:

http://www.nxp.com/assets/documents/data/en/user-guides/PINS_Install_Guide1.pdf

I hope this information helps!

Regards,