Pin Compatibility between Solo and SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Compatibility between Solo and SoloX

1,750 Views
amitjain
Contributor I

Hello,

Are iMX6 Solo and iMX6 SoloX are pin compatible?

If we replace iMX6 Solo with iMX6 SoloX will there be any changes in existing BSP for iMX6 Solo?

Thanks,

Amit Jain

Labels (2)
0 Kudos
Reply
2 Replies

1,601 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

I am afraid they are not pin compatible, in general recommended to check

AN4815 i.MX 6SoloX Migration Guide Migrating from i.MX 6Solo to i.MX 6SoloX

cache.freescale.com/files/32bit/doc/app_note/AN4815.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,601 Views
amitjain
Contributor I

Dear Igor,

Thanks for your reply.

Regards,

Amit Jain

0 Kudos
Reply