Pin Compatibility between Solo and SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin Compatibility between Solo and SoloX

1,748件の閲覧回数
amitjain
Contributor I

Hello,

Are iMX6 Solo and iMX6 SoloX are pin compatible?

If we replace iMX6 Solo with iMX6 SoloX will there be any changes in existing BSP for iMX6 Solo?

Thanks,

Amit Jain

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,599件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Amit

I am afraid they are not pin compatible, in general recommended to check

AN4815 i.MX 6SoloX Migration Guide Migrating from i.MX 6Solo to i.MX 6SoloX

cache.freescale.com/files/32bit/doc/app_note/AN4815.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,599件の閲覧回数
amitjain
Contributor I

Dear Igor,

Thanks for your reply.

Regards,

Amit Jain

0 件の賞賛
返信