Perf Test Failing on IMX6dl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Perf Test Failing on IMX6dl

1,729件の閲覧回数
vm18553
Contributor II

Perf test failing with following error,

bash-3.2# perf test
1: vmlinux symtab matches kallsyms                        : FAILED!
6: Validate PERF_RECORD_* events & perf_sample fields     : FAILED!
16: Try 'import perf' in python, checking link problems    : FAILED!
17: Test breakpoint overflow signal handler                : FAILED!
18: Test breakpoint overflow sampling                      : FAILED!
19: Test number of exit event of a simple workload         : FAILED!
21: Test object code reading                               : FAILED!

When I ran

bash-3.2# perf test -v 1
 1: vmlinux symtab matches kallsyms                        :
--- start ---
test child forked, pid 194
Looking at the vmlinux_path (7 entries long)
Couldn't find a vmlinux that matches the kernel running on this machine, skipping test
test child finished with 254
---- end ----
vmlinux symtab matches kallsyms: FAILED!

I have attached complete test log.

I found this https://forum.odroid.com/viewtopic.php?f=8&t=1581 where it mentioned after kernel version  3.6 perf is broken.

Have anyone tried to do perf testing on IMX6dl board?

 

Regards,

Vishnu

Original Attachment has been moved to: perf-test.log.zip

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,524件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vishnu

one can try with nxp releases on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

in general, as this is specific kernel issue it may be posted on kernel mail list

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信