Parallel interface camera module for MCIMX6Q - SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parallel interface camera module for MCIMX6Q - SDB

3,805件の閲覧回数
sathyanarayanan
Contributor I

Hi 

   In MCIMX6Q - SDB evaulation kit to interface the camera module parallel interface(DVP) and MIPI is provided. Pls suggest the camera module which able to connect with MCIMX6Q - SDB Parallel(DVP) interface connector. 

Thanks in advance 

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

3,274件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sathyanarayanan

it is OV5642, p.8 spf-27392 Sabre schematic

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,274件の閲覧回数
sathyanarayanan
Contributor I

Hi can you pls specify the exact part no of the module. pls note it should be mated with J9.

0 件の賞賛
返信

3,274件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,274件の閲覧回数
mbogenschuetz
Contributor I

Does anyone know a matching replacement board for the above mentioned parallel camera OV05642-MRSL-A01A ?

The OV05642-MRSL-A01A is discontinued and cannot be bought anymore as far as I can see.

(see https://www.ovt.com/download/datasets/6355/2QF14%20PDN%20Notification%202013%200930.pdf )

0 件の賞賛
返信