PTN5110 - iMX6UL - Kernel 5.15 - Device Tree Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PTN5110 - iMX6UL - Kernel 5.15 - Device Tree Configuration

5,212 次查看
screen-cleaner
Contributor I

Same Hardware, new Kernel

We are trying to update to the new Kernel 5.15.32 (old Kernel 4.19.72) but the USB-PD Chip (PTN5110) just does not work:

When we start the module tcpci with our Device Tree (see below) we get the following messages:

devel@europa:/usr/lib/modules/5.15.32+g4122737b2fca$ sudo modprobe tcpci
[  139.282440] OF: graph: no port node found in /soc/bus@2100000/i2c@21f8000/ptn5110@50
[  139.332044] OF: graph: no port node found in /soc/bus@2100000/i2c@21f8000/ptn5110@50/connector
[  139.341524] OF: graph: no port node found in /soc/bus@2100000/i2c@21f8000/ptn5110@50/connector

We did try to specify the port but were unlucky so far (nothing seams to work and we are trying for a few weeks now). The DT below worked wonderful in the old kernel but not the new one.
After loading the module we see some communication over the I2C port and everything seams to work fine. As soon as we plug in a USB connection the Kernel gets flooded with IRQ requests (or so it seams). The I2C bus is filled with data exchange and none of the consoles are reacting to any keystroke. After unplugging the USB connection the system reacts normal again. (the system seams to be blocked completely)

Our device tree:

/ {
	regulators {
		compatible = "simple-bus";
		#address-cells = <1>;
		#size-cells = <0>;

		reg_usb_otg1_vbus: regulator@2 {
			compatible = "regulator-fixed";
			reg = <2>;
			regulator-name = "usb_otg1_vbus";
			pinctrl-names = "default";
			pinctrl-0 = <&pinctrl_usb_otg1_vbus>;
			regulator-min-microvolt = <5000000>;
			regulator-max-microvolt = <5000000>;
			gpio = <&gpio2 8 GPIO_ACTIVE_HIGH>;
			enable-active-high;
			status = "okay";
		};
	};
};

&usbotg1 {
	/*pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_usbotg1>;*/
	dr_mode = "otg";
	status = "okay";
	disable-over-current;
	vbus-supply = <&reg_usb_otg1_vbus>;
};

&i2c4 {
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c4>;
	status = "okay";

	usb_pd: ptn5110@50 {
		compatible = "nxp,ptn5110";
		reg = <0x50>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_usb_pd>;
		interrupt-parent = <&gpio2>;
		interrupts = <11 IRQ_TYPE_LEVEL_LOW>;
		wakeup-source;

		usb_con: connector {
			compatible = "usb-c-connector";
			label = "USB-C";
			data-role = "dual";
			power-role = "dual";
			try-power-role = "sink";
			source-pdos = <PDO_FIXED(VSAFE5V, 2000, PDO_FIXED_USB_COMM | PDO_FIXED_DUAL_ROLE)>;
			sink-pdos = <PDO_FIXED(VSAFE5V, 2000, PDO_FIXED_USB_COMM | PDO_FIXED_DUAL_ROLE)
                                     //PDO_FIXED(VSAFE5V, 3000, 0)
                                     //PDO_FIXED(9000, 3000, 0)
                                     PDO_FIXED(12000, 3000, 0)
                                     PDO_FIXED(20000, 3000, 0)>;
                                     //PDO_FIXED(20000, 5000, 0)>;
			op-sink-microwatt = <10000000>;

		};
	};
};

&iomuxc {
	pinctrl_i2c4: i2c4grp {
		fsl,pins = <
			MX6UL_PAD_UART2_TX_DATA__I2C4_SCL	0x4001b8b0
			MX6UL_PAD_UART2_RX_DATA__I2C4_SDA	0x4001b8b0
		>;
	};

	pinctrl_usb_pd: usbpdgrp {
		fsl,pins = <
			MX6UL_PAD_ENET2_TX_DATA0__GPIO2_IO11	0x0001b020 /* Alert Interrupt */
			MX6UL_PAD_ENET2_TX_CLK__GPIO2_IO14		0x0001b020 /* Fault Interrupt */
		>;
	};

	pinctrl_usb_otg1_vbus: usbotg1 {
		fsl,pins = <
			MX6UL_PAD_ENET2_RX_DATA0__GPIO2_IO08	0x000000b9
			MX6UL_PAD_ENET2_RX_DATA1__USB_OTG1_OC	0x000010b0
		>;
	};
};

 

标签 (4)
0 项奖励
回复
8 回复数

5,079 次查看
screen-cleaner
Contributor I

So I did find out that the Chip goes into Fault every time I plug in a USB Connection. (It comes out of the Fault as soon as I unplug the USB)

On the I2C Bus I see that the Kernel Module keeps trying to reset the Fault flag without success.

I see a repeating pattern of:

  • 0x50 Write 0x10
  • 0x50 Read 0x00 0x02
  • 0x50 Write 0x10 0x00 0x02

As I wrote, the chip was working fine with the old Kernel 4.19.72 but not with the new Kernel 5.15.68.

If someone could tell me what is going wrong I would be very thankful.

0 项奖励
回复

5,177 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

The PTN5110 bindings for IMX6UL are the same that the IMX8MM, you can try this:

 

ptn5110: tcpc@50 {
		compatible = "nxp,ptn5110";
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_typec1>;
		reg = <0x50>;
		interrupt-parent = <&gpio2>;
		interrupts = <11 8>;
		status = "okay";

		port {
			typec1_dr_sw: endpoint {
				remote-endpoint = <&usb1_drd_sw>;
			};
		};

		typec1_con: connector {
			compatible = "usb-c-connector";
			label = "USB-C";
			power-role = "dual";
			data-role = "dual";
			try-power-role = "sink";
			source-pdos = <PDO_FIXED(5000, 3000, PDO_FIXED_USB_COMM)>;
			sink-pdos = <PDO_FIXED(5000, 3000, PDO_FIXED_USB_COMM)
				     PDO_VAR(5000, 20000, 3000)>;
			op-sink-microwatt = <15000000>;
			self-powered;
		};
	};

 

0 项奖励
回复

5,135 次查看
screen-cleaner
Contributor I

This reduces the messages from the module by 1 but the overall behaviour stays the same:

devel@ganymed:~$ sudo modprobe tcpci
[  297.071214] OF: graph: no port node found in /soc/bus@2100000/i2c@21f8000/ptn5110@50/connector
[  297.080634] OF: graph: no port node found in /soc/bus@2100000/i2c@21f8000/ptn5110@50/connector

 After loading the module and connecting the USB cable the system gets blocked by IRQ Requests from the chip and only response again after disconnecting the USB Connection.

0 项奖励
回复

5,131 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Ok, I see, could you please try with this?:

 

ptn5110@50 {
	compatible = "nxp,ptn5110";
	reg = <0x50>;
	interrupt-parent = <&gpio3>;
	interrupts =  IRQ_TYPE_LEVEL_LOW>;

	usb_con: connector {
		compatible = "usb-c-connector";
		label = "USB-C";
		data-role = "dual";
		power-role = "dual";
		try-power-role = "sink";
		source-pdos = <PDO_FIXED(5000, 2000, PDO_FIXED_USB_COMM)>;
		sink-pdos = <PDO_FIXED(5000, 2000, PDO_FIXED_USB_COMM)
			     PDO_VAR(5000, 12000, 2000)>;
		op-sink-microwatt = <10000000>;

		ports {
			#address-cells = <1>;
			#size-cells = <0>;

			port@1 {
				reg = <1>;
				usb_con_ss: endpoint {
					remote-endpoint = <&usb3_data_ss>;
				};
			};
		};
	};
};
0 项奖励
回复

5,115 次查看
screen-cleaner
Contributor I

Using this configuration does not change the faulty behaviour. Maybe it is not even a Problem of the Ports but the interrupt configuration:

As soon as I attach a USB Cable it seams to me as if the module can not resolve the interrupt request of the device. Do you see something wrong with that part of the configuration?

0 项奖励
回复

5,120 次查看
screen-cleaner
Contributor I

In the Documentation of the Kernel (https://www.kernel.org/doc/Documentation/devicetree/bindings/connector/usb-connector.yaml), we found this:

  ports:
    $ref: /schemas/graph.yaml#/properties/ports
    description: OF graph bindings modeling any data bus to the connector
      unless the bus is between parent node and the connector. Since a single
      connector can have multiple data buses every bus has an assigned OF graph
      port number as described below.

    properties:
      port@0:
        $ref: /schemas/graph.yaml#/properties/port
        description: High Speed (HS), present in all connectors.

      port@1:
        $ref: /schemas/graph.yaml#/properties/port
        description: Super Speed (SS), present in SS capable connectors.

      port@2:
        $ref: /schemas/graph.yaml#/properties/port
        description: Sideband Use (SBU), present in USB-C. This describes the
          alternate mode connection of which SBU is a part.

    required:
      - port@0

 Are you sure, we should not just use port@0?

0 项奖励
回复

5,148 次查看
screen-cleaner
Contributor I

What is referenced with usb1_drd_sw?

port {
	typec1_dr_sw: endpoint {
		remote-endpoint = <&usb1_drd_sw>;
	};
};

 and does it in return have to reference the typec1_dr_sw endpoint?

0 项奖励
回复

5,143 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

I guess you refer this:

 

&usbotg1 {
	dr_mode = "otg";
	hnp-disable;
	srp-disable;
	adp-disable;
	usb-role-switch;
	disable-over-current;
	samsung,picophy-pre-emp-curr-control = <3>;
	samsung,picophy-dc-vol-level-adjust = <7>;
	status = "okay";

	port {
		usb1_drd_sw: endpoint {
			remote-endpoint = <&typec1_dr_sw>;
		};
	};
};

 As I said, the IC2 of IMX6UL is the same that IMX8MM, so you can refer here for review that part.

I hope I have answered your question. 

Best regards!

0 项奖励
回复