POR signal and Power-up sequence for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

POR signal and Power-up sequence for i.MX6

1,347 次查看
yuuki
Senior Contributor II

Dear all,

We want to use POR signal to reset i.MX6 during system working.
Is the POR signal able to be asserted while all power supplies to i.MX6 are stable?

Does i.MX6 need Power up sequence when POR signal is asserted?

Best Regards,
Yuuki

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,084 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes power up sequence should be followed when POR signal is asserted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复