PMIC PF3000 datasheet Rev. 9.0, 8/2017 Documentation Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC PF3000 datasheet Rev. 9.0, 8/2017 Documentation Issue

1,118件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hello NXP Community,

 

I just want to inform you about a typo on the PMIC PF3000 datasheet Rev. 9.0, 8/2017.

On page 4 of the document claims that you can get 0.9V from VREFDDR:

 pastedImage_1.png

 

However, on page26 the datasheet claims that VINREFDDR maximum voltage is 1.65V being 0.15V below the voltage needed (1.8V) and below the claim from page 4.

 

pastedImage_3.png

 

 Page 26 is correct (Max VREFDDR is 1.65V), so the max VREFDDR you can get with the PF3000 is:

VREFDDR = VINREFDDR/2

VREFDDR = 1.65V / 2

VREFDDR = 0.825V

 

This issue has already reported to the Apps Engineers and should be corrected for the next revision of the datasheet.

 

- Jose

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)