Hi Weidong,
Thanks for your reply. The said design is part of the bigger system and this is a module in it and has input power that is 3.3V only. I do not have any option to increase the voltage. Is there any other alternative chip available.
WDI pin is showing low only.
I have isolated all the loads from the chip completely to check if it was overloading. Now if I give 3.6V from an external source it tries to come up and goes down immediately.
Is the load necessary for the PMIC to come up.
with best regards,
S.Satyan