PICO IMX8MM Training Failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PICO IMX8MM Training Failed

2,046件の閲覧回数
orenrocco
Contributor I

I keep receiving this error on my PICO IMX8MM 

and I have used DDR Tool but I believe I do not have the correct calibration file.


U-Boot SPL 2018.03-f30a821e93af654f523c565b0f9aa1f35306d2e5+gf30a821e93 (Feb 16 2020 - 16:57:19 +0000)
power_bd71837_init
dram_init: LPDDR4 4GB
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2

Thanks for the help,

Best Regards, 

Oren A.

ラベル(1)
0 件の賞賛
返信
1 返信

1,931件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oren

PICO IMX8MM is technexion board and supported directly by technexion,

May be useful to look at its images and post issue on Issues · TechNexion/u-boot-edm · GitHub 

PICO‐IMX8MM · TechNexion/u-boot-edm Wiki · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信