PF3000 current limit behavior of SW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000 current limit behavior of SW

ソリューションへジャンプ
549件の閲覧回数
Arcard334
Contributor I

Dear community,

 

I am considering using a device with the PF3000 built in. According to the datasheet, SW2 has a current limit during a short circuit, but I don't fully understand its specific operation.

For example, does it repeat 2 seconds OFF and 0.1 seconds ON, or does it stop outputting entirely until the short circuit is resolved?
Additionally, how long does the current limit last after a short circuit occurs?


Best Regards,
Kinosita

0 件の賞賛
返信
1 解決策
523件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

SW2 has an overcurrent sense bit (SW2FAULTS), it is asserted when SW2 above current limit. It takes 8 ms to detect the over current consumption.

SW2FAULTI register is set to 1 when the SW2 regulator is in current limit protection. This flag can only be cleared by writing a 1 to recover the SW2 output. Writing a 0 has no effect.

Best regards.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
524件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

SW2 has an overcurrent sense bit (SW2FAULTS), it is asserted when SW2 above current limit. It takes 8 ms to detect the over current consumption.

SW2FAULTI register is set to 1 when the SW2 regulator is in current limit protection. This flag can only be cleared by writing a 1 to recover the SW2 output. Writing a 0 has no effect.

Best regards.

0 件の賞賛
返信
500件の閲覧回数
Arcard334
Contributor I

Hi, JorgeCas.

 

Thank you for your reply.

So, it shuts down 8 milliseconds after detecting a short-circuit current.

 

Thank you for the information.