PF3000 PMIC 5V powered

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000 PMIC 5V powered

1,453件の閲覧回数
patrickoreilly
Contributor I

Hi, I want to use a pf3000 pmic on my imx6ul design. It will not be battery backed up. V supply will be 5V, so that means I will be using the VPWR input pin. In all reference designs I have come across, the VIN pin (<4.5V) is also used, and a FET is used to switch between inputs. I presume I can leave this FET out?

Also I notice on reference designs, the SW and LDO regs are tied to the <4.5V source. Are the inputs to these regulators not connected to the VIN/VPWR pin already?

Thanks

Patrick

0 件の賞賛
返信
1 返信

1,324件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patrick

for 5V fet should be used according to Table 2. Pin definitions, also
VLDO inputs are not connected to VIN/VPWR by default
http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信