PF3000 / PF3001

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF3000 / PF3001

1,499 次查看
ricardoferreira
Contributor II

Hi,

In the freescale website there on the PMIC PF3000/30001 there is the possibility to request samples for several PMICs.

For instance, the MC34PF3000A0EP and the MC32PF3000A6EP say that they are compatible with i.MX6UL.

Does it means that there is a default code on the PMIC that makes it compatible directly with the i.MX6UL without the need of flashing a new code?

Thank you very much in advance

Regards,

Ricardo F.

标签 (2)
标记 (3)
1 回复

1,278 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ricardo

right, one can use A6,A7 options without additional programming

according to Table 1

http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------