PF3000 A2 version setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 A2 version setting

1,562 Views
frankyhsu
Contributor III

Hi Support,

We are using A0 version and program it to fit LPDDR3 application by myself. Now, we are planing to use A2 version but we are not sure what is the SW2 (1.8V) and SW3 (1.2V) DVS clk setting. We want to support the rising time higher than 100uS so we set the DVS clk to be 6.25mV/us. Do you help to check it?

And, if the setting is 12.5mV/us, the only way for us is to use A0 version and find 3rd part help to program it for mass production?

Labels (2)
0 Kudos
Reply
1 Reply

1,482 Views
guoweisun
NXP TechSupport
NXP TechSupport

Thanks for your interesting in NXP prodcucts.

The DVS is setting 12.5mV/us about A2 version,you can select A0 version then do a OTP by youself.

Thanks!

0 Kudos
Reply