PF0100 Programming Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 Programming Error

4,466件の閲覧回数
legbam5
Contributor I

The verify after programming shows errors. 

legbam5_LEGNB0555_2019-07-15-000042.jpg

After repowering and verify "NO programming erros" appears.

I don't understand it.

The error code 0x05 in fuse bank 0xE3 is not descibed in AN4536.

ラベル(1)
0 件の賞賛
返信
1 返信

4,383件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Can you please check if the PMIC is already programmed before you try to program it, please?

 

You can do this by clicking on the “Blank Check” button.

 

If the PMIC is already programmed, it will not be possible to re-program it and this could be the cause of the programming errors you are seen.

0 件の賞賛
返信