PCM INTERFACE TO IMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCM INTERFACE TO IMX6UL

1,404 Views
dhanushdc
Contributor I

hi, I am using imx6ulrm processor .i am using external codec and bc127 Bluetooth module. can I connect SAI (SYNCHRONOUS AUDIO INTERFACE) to bc127 Bluetooth module PCM pins pcm_in,pcm_out,pcm_mclk and pcm_sync and operate 

Labels (1)
0 Kudos
Reply
1 Reply

1,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi DHANUSH

"pcm" is quite generic word for many timing protocols, please provide

bc127 audio interface waveforms. For supported sai formats please look at AN4486

http://cache.freescale.com/files/microcontrollers/doc/AN4486.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply