PCIe endpoint driver with DMA support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe endpoint driver with DMA support

2,933 Views
shabbirlimdiwal
Contributor I

Hi,

Is i.mx6 quad validated with PCIe end point mode in Linux? Is DMA implementation already available for PCIe end point?

We have a high throughput requirement (output 720P30, YUV422) over PCIe. Will i.mx6 quad be sufficient enough to do so?

Thanks and Regards,

Shabbir

Tags (2)
0 Kudos
Reply
1 Reply

2,202 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shabbir

yes it is validated

i.MX6Q PCIe EP/RC Validation System

please also check attached document sect.35.5 i.MX 6Quad SD PCIe RC/EP Validation System

included in L3.0.35_4.1.0_ER_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply