PCIe EP DMA write to i.MX6 RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe EP DMA write to i.MX6 RAM

1,417 Views
egabay1
Contributor I

Hi,

Under the following conditions:

-. i.MX6 configured as PCIe RC

- The i.MX6 is connected to PCIe EP

- The EP wants to perform DMA write operation to the I.MX6 RAM

Does this scenario supported?

Thanks,

Eyal

0 Kudos
Reply
1 Reply

1,289 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Eyal,

In EP's system, EP can access the reserved ddr memory    (default address:0x40000000) of PCIe RC's system, by the   interconnection between PCIe EP and PCIe RC. So I don´t see a problem.

Here is a link of a validation

i.MX6Q PCIe EP/RC Validation System 


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply