PCIe 1 on iMX8-QM MEK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe 1 on iMX8-QM MEK

411 Views
mhul1909
Contributor I

Looking at the schematics for the MEK, it appears that only PCIE_CTRL0 pins are routed to the M.2 connector and PCIE_CTRL1 pins are instead routed to the B2B connector. If I've understood correctly, this means a device connected via the M.2 interface will only be accessible through the PCIE 0 (A) instance. 

Is that correct? If so, how could I go about testing PCIE 1 (B)? Assume using NXP Linux kernel lf-6.1 with hsio-cfg set such that one lane each of phyx2 is assigned to PCIE instances 0 and 1. 

On a related topic, I'm not able to find a schematic for the MCIMX8-8X-BB base board. Would appreciate being pointed in its direction. 

Tags (3)
0 Kudos
Reply
1 Reply

390 Views
jimmychan
NXP TechSupport
NXP TechSupport

The base board schematic could be downloaded from here:

i.MX8 MEK Base Board Design Files

https://www.nxp.com/webapp/Download?colCode=iMX8MEK_BaseBoard_DF

0 Kudos
Reply