PCIMX7D3DVK10SA Current consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIMX7D3DVK10SA Current consumption

1,166 Views
ranjithraviprak
Contributor I

hi,

We are using PCIMX7D3DVK10SA in one of our designs. I am looking for current consumption values for all the voltage rails in the processor. Datasheet says most of these values are TBD. I need these numbers for proper DC-DC design.

Ranjith

0 Kudos
Reply
1 Reply

1,122 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

as this is preproduction part all info about it can be obtained from local FAE.

Also one can try to enter Service Request to get preliminary data.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply