Output transient response

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output transient response

1,222 Views
ban45
Contributor III

NVCC_DRAM is 1.35V .

i.MX6 solo is input range of the NVCC_DRAM 1.283V to 1.450V.

Due to Output transient response, NVCC_DRAM will be less than 1.283V between 20us and 40us.

When using MMPF0100(SW3B) The output voltage tolerance is ±3% and the transient response is 50mV(max).

The maximum value is 6% or more 、NVCC_DRAM is  1.283V or less.

Is it necessary to consider the effect of transient response?

Is there any problem with 20us and 40us?

0 Kudos
Reply
1 Reply

1,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori 

NVCC_DRAM limits, defined in Table 8. Operating Ranges

i.MX 6Solo/6DualLite Applications Processors for Consumer Products

should not be exceeded even during transients.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply