Ota zip File isgetting updated with boot.img,bootloader.imgThu, Jul 14 2011 23:58:32 and META_INFO with may 19 2017 with in imx6dq on andriod MARSHMELLOW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ota zip File isgetting updated with boot.img,bootloader.imgThu, Jul 14 2011 23:58:32 and META_INFO with may 19 2017 with in imx6dq on andriod MARSHMELLOW

2,813件の閲覧回数
ayyappadasps
Contributor II

i am following the below steps

please help me???????????

OTA update

1. TO build the source we are using the script file ->android_build.sh

2. To build the ota package i am following the below commands


source build/envsetup.sh
lunch sabresd_6dq-user
make

3.After the make success i am doing the following for getting ota file


make otapackage

make PRODUCT=sabresd_6dq-user otapackage -j4

then obtainment is below

-rw-rw-r-- 1 zumi-02 zumi-02 8865064 Jul 14 2011 boot.img
-rw-rw-r-- 1 zumi-02 zumi-02 445440 Jul 14 2011 bootloader.img
-rw-rw-r-- 1 zumi-02 zumi-02 15407 Jul 14 2011 file_contexts
drwxrwxr-x 3 zumi-02 zumi-02 4096 May 19 19:18 META-INF
-rw-rw-r-- 1 zumi-02 zumi-02 536698880 Jul 14 2011 system.new.dat
-rw-rw-r-- 1 zumi-02 zumi-02 0 Jul 14 2011 system.patch.dat
-rw-rw-r-- 1 zumi-02 zumi-02 345 Jul 14 2011 system.transfer.list

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,559件の閲覧回数
ayyappadasps
Contributor II

Hi jimmychan

                        i followed the same procedure in question 30 .but i am not getting any updated zip file

0 件の賞賛
返信

2,557件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Attached is the FAQ for Android BSP. you can find the OTA information in section 30.

0 件の賞賛
返信