Optimizing power consumption in IMX platforms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Optimizing power consumption in IMX platforms

1,387 Views
lyfsci
Contributor III

Hi Experts,

Is there any white paper document on the power optimization in the iMX platforms for Linux and android ?

What are all the factors I should consider in Linux to start optimizing the power ?

Any general guidelines ?

Regards,

Lyf

Labels (2)
0 Kudos
Reply
1 Reply

1,141 Views
Yuri
NXP Employee
NXP Employee

Lyf,

  Please refer to section 4 (Reducing power consumption) of app note AN4509

(i.MX 6Dual/6Quad Power Consumption Measurement).

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply