Optimizing power consumption in IMX platforms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Optimizing power consumption in IMX platforms

1,378件の閲覧回数
lyfsci
Contributor III

Hi Experts,

Is there any white paper document on the power optimization in the iMX platforms for Linux and android ?

What are all the factors I should consider in Linux to start optimizing the power ?

Any general guidelines ?

Regards,

Lyf

ラベル(2)
0 件の賞賛
返信
1 返信

1,132件の閲覧回数
Yuri
NXP Employee
NXP Employee

Lyf,

  Please refer to section 4 (Reducing power consumption) of app note AN4509

(i.MX 6Dual/6Quad Power Consumption Measurement).

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信