Operating System on imx6ulevk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Operating System on imx6ulevk board

1,499件の閲覧回数
nitigupta
Contributor I


Hello All,

Currently I am working on imx6ulevk board having configuration "140kB RAM, 1MB ROM, 524 MHz One core cortex A7 with Neon & 1MB QSPI flash(external)". I want to run either linux or rtos on it but I am not getting which linux or rtos I should use on it. Is it feasible to run linux on it. Also I am confused which rtos is best possibly work with it.

Any help in this regard is highly appreciated.

Thanks,

Niti Gupta

0 件の賞賛
返信
1 返信

1,296件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niti

for linux one can look at i.MX6UL product page:

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul)

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

i.MX6UltraLite Evaluation Kit|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信