Hi,
I’ve downloaded CST 4.0.1 (Code Signing Tool) from NXP, and while reviewing the documentation in the docs folder—specifically UG10106—I came across section 3.1.1, which mentions that CST supports Ubuntu 22.04 and requires OpenSSL 3.2.0.
However, my current Ubuntu 22.04 system has OpenSSL 3.0.2 installed. I'm concerned that upgrading to OpenSSL 3.2.0 might break existing system dependencies. Do I really need to upgrade OpenSSL to use CST? If so, what’s the safest way to do it without affecting my system?
I’ve also attached a screenshot from UG10106 for reference.
Thanks,
Kartheek