OpenSSL Library for Linux imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenSSL Library for Linux imx

2,691 Views
niranjanbc
Contributor IV

hi 

i am looking to use latest openssl library(1.1.0g) in Linux imx6 bsp, how include that.

do you have recipes to include the latest openssl.

in openssl website i see latest is openssl.1.1.0g

currently i see we are using openssl.1.0.2d in linux bsp for imx6solox.

i tried specifying  preferred version in local.conf and machine.conf, i get warning messages saying version not available.  

0 Kudos
Reply
1 Reply

2,222 Views
b36401
NXP Employee
NXP Employee

At this moment we have no plan to migrate to openssl 1.1.0.

Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply