OpenMAX IL support for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenMAX IL support for i.MX6

2,364件の閲覧回数
kirgene
Contributor II

Hello,

I have a multimedia software based on OpenMAX IL that runs on Linux.

I'd like to know if there any support for OpenMAX from i.MX drivers so that I can easily port this software to i.MX platform?

Thanks.

0 件の賞賛
返信
1 返信

1,635件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yevhen

i.mx extended multimedia feature package provides support

for OMXPlayer framework for android, not for linux.

Board Support Packages (27)

IMX6-L500-100-ANDROID-SOURCE-BSP (REV L5.0.0_1.0.0)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite and

i.MX6SX Android L5.0.0_1.0.0 BSP, Source Code for BSP and Codecs.

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信