OpenJDK 64-Bit Server VM warning:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenJDK 64-Bit Server VM warning:

ソリューションへジャンプ
27,792件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

Got following error while building android 9 automotive for IMX8 board. Please provide the fix for it,

OpenJDK 64-Bit Server VM warning: INFO: os::commit_memory(0x0000000761500000, 635437056, 0) failed; error='Not enough space' (errno=12)

 

Resolved by reboot. But, I need permanent solution.

 

 

Thanks & Regards,

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
27,783件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

The following suggestions are for your reference:
1. Linux Ubuntu host has at least 16GB Memory.
2. Linux Ubuntu host has at least 300GB hard disk space.
3. If the ubuntu host has 16GB memory, you can compile with 4 threads at most; if the compilation threads are greater than 4, there may still be insufficient memory

Hope above information is helpful to you.

Have a nice day!

B.R,

weidong

元の投稿で解決策を見る

2 返答(返信)
27,784件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

The following suggestions are for your reference:
1. Linux Ubuntu host has at least 16GB Memory.
2. Linux Ubuntu host has at least 300GB hard disk space.
3. If the ubuntu host has 16GB memory, you can compile with 4 threads at most; if the compilation threads are greater than 4, there may still be insufficient memory

Hope above information is helpful to you.

Have a nice day!

B.R,

weidong

27,760件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you weidong_sun

 

You are right my local desk D have less than the 300 GB. after freed I got resolved from this.

Linux Ubuntu host has at least 300GB hard disk space.

 

Regards,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信