[OpenGL ES3] Does integer texture are supported on imx6q GPU?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[OpenGL ES3] Does integer texture are supported on imx6q GPU?

2,963件の閲覧回数
anthonygonin
Contributor II

Hi all,

I work on a program using OpenGL ES3.0 and I would like to do bit-wise shift on texture data. I can't render anything when I specify my texture as GL_RGB8UI and GL_RGB_INTEGER. But for GL_RGB8 and GL_RGB it works, I render an image but I can't perform a bit-wise shifting because it is not integer's data.


So I am asking if integer texture is supported on this gpu. I saw that an extension exists for this but it is not listed in the imx6 Graphics User Guide.

Thanks for your help.

Anthony

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,668件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Anthony, 

bitwise texture data with GL_RGB8UI and GL_RGB_INTEGER should works . however make sure that you are not using fixed functions, for fixed functions you should use shaders. In any case it looks like GL_RGB8 and GL_RGB works is because you are  rendering textures images at 16-bit alignment. 

Regards

0 件の賞賛
返信

2,668件の閲覧回数
anthonygonin
Contributor II

Hi, and sorry for my late answer (I got problem on other project).

I think my problem could not be one but just a missing knowledge of openGL, but I will describe what I really want to do and my problem.

I would like to access texture value in the fragment shader to do bitwise operations. More precisely I would like to transform Input(R,G,B) to Output(R, G, (R&0xF0)|(G&0xF0)>>4).

To do this I would like to access my texture value as integer and not float as it is by default.

To do this I use a FBO and I configure it like this : 

    glGenFramebuffers(1, &m_uiFrameBufferObject);
    glBindFramebuffer(GL_FRAMEBUFFER, m_uiFrameBufferObject);

   

    glGenTextures(1, &m_uiTextureFB);
    glBindTexture(GL_TEXTURE_2D, m_uiTextureFB);

   

    glTexImage2D(GL_TEXTURE_2D, 0, GL_RGB8UI, WIDTH, HEIGHT, 0, GL_RGB_INTEGER, GL_UNSIGNED_BYTE, nullptr);

   
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MIN_FILTER, GL_NEAREST);
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MAG_FILTER, GL_NEAREST);

   
    glFramebufferTexture2D(GL_FRAMEBUFFER, GL_COLOR_ATTACHMENT0, GL_TEXTURE_2D, m_uiTextureFB, 0);

And then I do a render to texture with a texture configure like this : 

    glGenTextures(1, &m_uiTextureId);
    glBindTexture(GL_TEXTURE_2D, m_uiTextureId);
    glTexImage2D(GL_TEXTURE_2D, 0, GL_R8, WIDTH_IN, HEIGHT_IN, 0, GL_RED, GL_UNSIGNED_BYTE, ucImage);

When I check the frame buffer, I have the error : GL_FRAMEBUFFER_INCOMPLETE_ATTACHMENT

And it  works if my texture is GL_RGB and not GL_RGB8UI. But when I read the open gl es 3.0 spec it is written that GL_RGB8UI is not color renderable so this is why it doesn't work.

I will try with GL_RGBA8UI which is color renderable and I see if it's OK.

Thanks for your time.

0 件の賞賛
返信