OV5640 Interfacing to LPC4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5640 Interfacing to LPC4357

1,526 Views
sudheerkumardor
Contributor I

Hi every one,

   I am trying to interface 0V5640 camera sensor with LPC4357. I am able to communicate with the sensor using SCCB(i2c). I  just want to capture the JPG image, i did the required configurations to capture image(DVP). Even i did configurations for DVP it is still giving output in MIPI lanes only. can any one suggest required configurations to capture the data.

0 Kudos
Reply
1 Reply

1,370 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello sudheer,

    On LPC4357, there are no MIPI-CSI2 & CSI(camer sensor interface) interface for recieving camera data, so you can't connect OV5640 with MIPI-CSI2 interface to LPC4357 directly, so your application is spectial, about hardware connections, you can evaluate following advice:

pastedImage_1.png

Then you can get 1 Frame picture with JPG format through USB port in software!

Hope above advice can help you!

Best Regards,

Weidong

0 Kudos
Reply