OPENGLES 3.0 support for imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OPENGLES 3.0 support for imx6

1,343 Views
ganesank
Contributor III

Hi,

I am not sure whether OPENGLES3.0 is supported for imx6 Dual core. When I build with Yocto I see only es20 folder under /opt/viv_samples/ folder. Has anyone used OPENGLES3.0 with Vivante?

Regards,

Ganesan. K

Labels (2)
0 Kudos
Reply
1 Reply

1,107 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ganesan,

Unfortunately the i.MX6 Family does not support OPENGLES 3.0  at least not with Hardware Accelerated. This means the GPU it is not prepared at this moment to support OpenGLES 3.0 .  But we are planning to have the i.MX8 which it is going to have this support.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply