Nothing visible on VGA after booting WEC7 image on QSB START-R board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nothing visible on VGA after booting WEC7 image on QSB START-R board

1,193件の閲覧回数
surjitkumar
Contributor II

I downloaded the image of the WEC7 from adeneo link and tried to boot the QSB START-R board by following the steps given in “FREESCALE_iMX53_QSB_WEC7_user_guide_V131.pdf”.

I have tried to boot the Start-R board by image "........\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel" by using uSD card by using following commands

    cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53

cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\nk.nb0 -d H -imx53 “

After this command if i insert uSD card in START-R board by connecting the power cable and VGA cable, nothing is visible on VGA.


ラベル(2)
0 件の賞賛
返信
1 返信

640件の閲覧回数
martincoster
Contributor II

Hi,

We are also having the exact same issue - everything seems to be starting up OK via the terminal output, but no VGA video output. We are using Freescale MCIMX53-START-R Rev D0. We do not have any touchscreen LCD card. We are using the HDMI daughter board, but we are looking at the VGA output.

Many thanks,

Martin Coster

nkcfimager.jpg

ebootCfimager.jpg

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb

BSP Clock Configuration:

    OSC         =   24000000 Hz

    PLL1        =  800000000 Hz

    PLL2        =  600000000 Hz

    PLL3        =  400000000 Hz

    PLL4        =  595000000 Hz

    LP_APM      =   24000000 Hz

    ARM         =  800000000 Hz

    AXI_A       =  300000000 Hz

    AXI_B       =  200000000 Hz

    EMI_SLOW    =  120000000 Hz

    AHB         =  120000000 Hz

    IPG         =   60000000 Hz

    PERCLK      =    8000000 Hz

    CKIL_SYNC   =      32768 Hz

    DDR         =  300000000 Hz

    ARM_AXI     =  200000000 Hz

    IPU_HSP     =  200000000 Hz

    VPU_AXI     =  200000000 Hz

    GPU         =  200000000 Hz

    GPU2D       =  200000000 Hz

    DEBUG_APB   =  200000000 Hz

    ENFC        =   30000000 Hz

    USBOH3      =   66666666 Hz

    ESDHC1      =  100000000 Hz

    ESDHC2      =  100000000 Hz

    ESDHC3      =  100000000 Hz

    ESDHC4      =  100000000 Hz

    UART        =   24000000 Hz

    SSI1        =    6000000 Hz

    SSI2        =    6000000 Hz

    SSI3        =    6000000 Hz

    SSI_EXT1    =   24000000 Hz

    SSI_EXT2    =   19047619 Hz

    USB_PHY     =   24000000 Hz

    TVE_216_54  =  297500000 Hz

    DI0         =   50000000 Hz

    DI1         =  297500000 Hz

    VPU_RCLK    =   24000000 Hz

    SSI_LP_APM  =   24000000 Hz

    SPDIF_XTAL  =   24000000 Hz

    LDB_DIO     =  595000000 Hz

    LDB_DI1     =  595000000 Hz

    SPDIF0      =    1142857 Hz

    ESAI        =    3000000 Hz

    ESAI_HCKR   =          0 Hz

    ESAI_HCKT   =          0 Hz

    CAN         =   60000000 Hz

    FIRI        =   24000000 Hz

    CSI_MCLK1   =   25000000 Hz

    CSI_MCLK2   =   25000000 Hz

    ECSPI       =   66666666 Hz

    LPSR        =          0 Hz

    PGC         =    7500000 Hz

    ASRC        =   59500000 Hz

    IEEE_CEMX   =   40000000 Hz

    CKIH        =   22579200 Hz

    CKIH2       =          0 Hz

Microsoft Windows CE Bootloader Common Library Version 1.4 Built May 22 2013 18:39:43

OALMc34708PmicI2cInit: Trying to init PMIC I2C Interface

OALPmicInit: Trying to init I2C Interface

MC34708 Version code : 14

INFO: BoardID = 0xc03.

INFO: EVK RevA board is not detected, switch ddr clock to 400MHz.

INFO: Increasing CPU clock to 1.0 GHz.

Microsoft Windows CE Ethernet Bootloader 1.31 for MX53 EVK (May 23 2013 16:59:42)

Get The name for the external PHY is LAN8720

INFO: SBMR = 0x10c63d45.

INFO:  Bootloader launched from SD.

ESDHC[1] is being activated...

SD High Density card

SD: Switched to 4 bit mode

INFO: Initialized SD Card

ATA device is not present 0x0

WARNING: OEMPlatformInit: Failed to initialize ATA device.

NAND ID is 0x3f3f3f3f

NAND ID read out is 0x3f3f3f3f, doesn't meet 0xd52c which is expected.

Failed to initialize NandFmd.

WARNING: OEMPlatformInit: Failed to initialize NAND flash device.

SPIFMD_Init: Manufacturer ID = 0x0

SPIFMD_Init: Manufacturer ID is not supported yet

WARNING: OEMPlatformInit: Failed to initialize SPI device.

INFO: Loading boot configuration from SDHC

INFO: Successfully loaded boot configuration from SDHC

System ready!

Preparing for download...

Press [ENTER] to launch image stored in SD/MMC or [SPACE] to cancel.

Initiating image launch in 3 seconds. 2 seconds. 1 seconds. 0 seconds.

Launching flash image  ...

-BLMenu .

INFO: Using device name: 'MX539730'INFO: Reading NK image to SDHC (please wait)...

INFO: Copying NK image to RAM address 0xa0200000

INFO: Read is 1% complete

INFO: Read is 2% complete

INFO: Read is 3% complete

INFO: Read is 4% complete

INFO: Read is 5% complete

INFO: Read is 6% complete

INFO: Read is 7% complete

INFO: Read is 8% complete

INFO: Read is 9% complete

INFO: Read is 10% complete

INFO: Read is 11% complete

INFO: Read is 12% complete

INFO: Read is 13% complete

INFO: Read is 14% complete

INFO: Read is 15% complete

INFO: Read is 16% complete

INFO: Read is 17% complete

INFO: Read is 18% complete

INFO: Read is 19% complete

INFO: Read is 20% complete

INFO: Read is 21% complete

INFO: Read is 22% complete

INFO: Read is 23% complete

INFO: Read is 24% complete

INFO: Read is 25% complete

INFO: Read is 26% complete

INFO: Read is 27% complete

INFO: Read is 28% complete

INFO: Read is 29% complete

INFO: Read is 30% complete

INFO: Read is 31% complete

INFO: Read is 32% complete

INFO: Read is 33% complete

INFO: Read is 34% complete

INFO: Read is 35% complete

INFO: Read is 36% complete

INFO: Read is 37% complete

INFO: Read is 38% complete

INFO: Read is 39% complete

INFO: Read is 40% complete

INFO: Read is 41% complete

INFO: Read is 42% complete

INFO: Read is 43% complete

INFO: Read is 44% complete

INFO: Read is 45% complete

INFO: Read is 46% complete

INFO: Read is 47% complete

INFO: Read is 48% complete

INFO: Read is 49% complete

INFO: Read is 50% complete

INFO: Read is 51% complete

INFO: Read is 52% complete

INFO: Read is 53% complete

INFO: Read is 54% complete

INFO: Read is 55% complete

INFO: Read is 56% complete

INFO: Read is 57% complete

INFO: Read is 58% complete

INFO: Read is 59% complete

INFO: Read is 60% complete

INFO: Read is 61% complete

INFO: Read is 62% complete

INFO: Read is 63% complete

INFO: Read is 64% complete

INFO: Read is 65% complete

INFO: Read is 66% complete

INFO: Read is 67% complete

INFO: Read is 68% complete

INFO: Read is 69% complete

INFO: Read is 70% complete

INFO: Read is 71% complete

INFO: Read is 72% complete

INFO: Read is 73% complete

INFO: Read is 74% complete

INFO: Read is 75% complete

INFO: Read is 76% complete

INFO: Read is 77% complete

INFO: Read is 78% complete

INFO: Read is 79% complete

INFO: Read is 80% complete

INFO: Read is 81% complete

INFO: Read is 82% complete

INFO: Read is 83% complete

INFO: Read is 84% complete

INFO: Read is 85% complete

INFO: Read is 86% complete

INFO: Read is 87% complete

INFO: Read is 88% complete

INFO: Read is 89% complete

INFO: Read is 90% complete

INFO: Read is 91% complete

INFO: Read is 92% complete

INFO: Read is 93% complete

INFO: Read is 94% complete

INFO: Read is 95% complete

INFO: Read is 96% complete

INFO: Read is 97% complete

INFO: Read is 98% complete

INFO: Read is 99% complete

INFO: Read is 100% complete

INFO: Copy of NK completed successfully

Either card is not eSD2.1, or boot partition is not created yet

Download successful!  Jumping to image at 0x0 (physical 0x70200000)...

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0x8b

BSP Clock Configuration:

    OSC         =   24000000 Hz

    PLL1        = 1000000000 Hz

    PLL2        =  400000000 Hz

    PLL3        =  400000000 Hz

    PLL4        =  595000000 Hz

    LP_APM      =   24000000 Hz

    ARM         = 1000000000 Hz

    AXI_A       =  400000000 Hz

    AXI_B       =  200000000 Hz

    EMI_SLOW    =  133333333 Hz

    AHB         =  133333333 Hz

    IPG         =   66666666 Hz

    PERCLK      =    8000000 Hz

    CKIL_SYNC   =      32768 Hz

    DDR         =  400000000 Hz

    ARM_AXI     =  200000000 Hz

    IPU_HSP     =  200000000 Hz

    VPU_AXI     =  200000000 Hz

    GPU         =  200000000 Hz

    GPU2D       =  200000000 Hz

    DEBUG_APB   =  200000000 Hz

    ENFC        =   33333333 Hz

    USBOH3      =   66666666 Hz

    ESDHC1      =  100000000 Hz

    ESDHC2      =  100000000 Hz

    ESDHC3      =  100000000 Hz

    ESDHC4      =  100000000 Hz

    UART        =   24000000 Hz

    SSI1        =    6000000 Hz

    SSI2        =    6000000 Hz

    SSI3        =    6000000 Hz

    SSI_EXT1    =   24000000 Hz

    SSI_EXT2    =   19047619 Hz

    USB_PHY     =   24000000 Hz

    TVE_216_54  =  297500000 Hz

    DI0         =   50000000 Hz

    DI1         =  297500000 Hz

    VPU_RCLK    =   24000000 Hz

    SSI_LP_APM  =   24000000 Hz

    SPDIF_XTAL  =   24000000 Hz

    LDB_DIO     =  595000000 Hz

    LDB_DI1     =  595000000 Hz

    SPDIF0      =    1142857 Hz

    ESAI        =    3000000 Hz

    ESAI_HCKR   =          0 Hz

    ESAI_HCKT   =          0 Hz

    CAN         =   66666666 Hz

    FIRI        =   24000000 Hz

    CSI_MCLK1   =   25000000 Hz

    CSI_MCLK2   =   25000000 Hz

    ECSPI       =   66666666 Hz

    LPSR        =          0 Hz

    PGC         =    8333333 Hz

    ASRC        =   59500000 Hz

    IEEE_CEMX   =   40000000 Hz

    CKIH        =   22579200 Hz

    CKIH2       =          0 Hz

Windows CE Kernel for ARM (Thumb Enabled)

OEMInit:  silicon ?= 0x21

BoardID = 0xc03.

Setting 1.2v regulator PLL1P2 to 1.3v

PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

PID:00400002 TID:00510002 WARNING: SRTC was reset.

PID:00400002 TID:011A006E UsbHost : New Function [address(1) / layer(0)]

PID:00400002 TID:00A20026 OTG : Load HCD

PID:00400002 TID:00A20026 OTG : Unload HCD

PID:00400002 TID:00A20026 OTG : Load UFN

PID:00400002 TID:00A20026 UfnClientLib!UfnCheckPID: WARNING -- using MS reference platform VID/PID 0x045e/0x00ce (not allowed in shipping platforms)

PID:00400002 TID:03640026 WARNING: possible performance issue: timeInit() not called, calling it in timeSetEvent()PID:00400002 TID:03640026 Pin muxing for Display pins complete.

PID:00400002 TID:03640026 KeybdDriverInitializeEx: Layout Manager successfully initialized to  1

PID:00400002 TID:03640026 LayoutMgrActivateKeyboardLayout: Called with hkl = 0x00000409

PID:01D70026 TID:05C00006 MSIM: IM_ReadRegistry read KB 5

PID:05C20006 TID:04980036 Explorer(V2.0) taskbar thread started.

PID:00400002 TID:03A20006 NDISPWR:: Found adapter [FEC1]

0 件の賞賛
返信