I downloaded the image of the WEC7 from adeneo link and tried to boot the QSB START-R board by following the steps given in “FREESCALE_iMX53_QSB_WEC7_user_guide_V131.pdf”.
I have tried to boot the Start-R board by image "........\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel" by using uSD card by using following commands
cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53
cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\nk.nb0 -d H -imx53 “
After this command if i insert uSD card in START-R board by connecting the power cable and VGA cable, nothing is visible on VGA.
Hi,
We are also having the exact same issue - everything seems to be starting up OK via the terminal output, but no VGA video output. We are using Freescale MCIMX53-START-R Rev D0. We do not have any touchscreen LCD card. We are using the HDMI daughter board, but we are looking at the VGA output.
Many thanks,
Martin Coster
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
BSP Clock Configuration:
OSC = 24000000 Hz
PLL1 = 800000000 Hz
PLL2 = 600000000 Hz
PLL3 = 400000000 Hz
PLL4 = 595000000 Hz
LP_APM = 24000000 Hz
ARM = 800000000 Hz
AXI_A = 300000000 Hz
AXI_B = 200000000 Hz
EMI_SLOW = 120000000 Hz
AHB = 120000000 Hz
IPG = 60000000 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 300000000 Hz
ARM_AXI = 200000000 Hz
IPU_HSP = 200000000 Hz
VPU_AXI = 200000000 Hz
GPU = 200000000 Hz
GPU2D = 200000000 Hz
DEBUG_APB = 200000000 Hz
ENFC = 30000000 Hz
USBOH3 = 66666666 Hz
ESDHC1 = 100000000 Hz
ESDHC2 = 100000000 Hz
ESDHC3 = 100000000 Hz
ESDHC4 = 100000000 Hz
UART = 24000000 Hz
SSI1 = 6000000 Hz
SSI2 = 6000000 Hz
SSI3 = 6000000 Hz
SSI_EXT1 = 24000000 Hz
SSI_EXT2 = 19047619 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 297500000 Hz
DI0 = 50000000 Hz
DI1 = 297500000 Hz
VPU_RCLK = 24000000 Hz
SSI_LP_APM = 24000000 Hz
SPDIF_XTAL = 24000000 Hz
LDB_DIO = 595000000 Hz
LDB_DI1 = 595000000 Hz
SPDIF0 = 1142857 Hz
ESAI = 3000000 Hz
ESAI_HCKR = 0 Hz
ESAI_HCKT = 0 Hz
CAN = 60000000 Hz
FIRI = 24000000 Hz
CSI_MCLK1 = 25000000 Hz
CSI_MCLK2 = 25000000 Hz
ECSPI = 66666666 Hz
LPSR = 0 Hz
PGC = 7500000 Hz
ASRC = 59500000 Hz
IEEE_CEMX = 40000000 Hz
CKIH = 22579200 Hz
CKIH2 = 0 Hz
Microsoft Windows CE Bootloader Common Library Version 1.4 Built May 22 2013 18:39:43
OALMc34708PmicI2cInit: Trying to init PMIC I2C Interface
OALPmicInit: Trying to init I2C Interface
MC34708 Version code : 14
INFO: BoardID = 0xc03.
INFO: EVK RevA board is not detected, switch ddr clock to 400MHz.
INFO: Increasing CPU clock to 1.0 GHz.
Microsoft Windows CE Ethernet Bootloader 1.31 for MX53 EVK (May 23 2013 16:59:42)
Get The name for the external PHY is LAN8720
INFO: SBMR = 0x10c63d45.
INFO: Bootloader launched from SD.
ESDHC[1] is being activated...
SD High Density card
SD: Switched to 4 bit mode
INFO: Initialized SD Card
ATA device is not present 0x0
WARNING: OEMPlatformInit: Failed to initialize ATA device.
NAND ID is 0x3f3f3f3f
NAND ID read out is 0x3f3f3f3f, doesn't meet 0xd52c which is expected.
Failed to initialize NandFmd.
WARNING: OEMPlatformInit: Failed to initialize NAND flash device.
SPIFMD_Init: Manufacturer ID = 0x0
SPIFMD_Init: Manufacturer ID is not supported yet
WARNING: OEMPlatformInit: Failed to initialize SPI device.
INFO: Loading boot configuration from SDHC
INFO: Successfully loaded boot configuration from SDHC
System ready!
Preparing for download...
Press [ENTER] to launch image stored in SD/MMC or [SPACE] to cancel.
Initiating image launch in 3 seconds. 2 seconds. 1 seconds. 0 seconds.
Launching flash image ...
-BLMenu .
INFO: Using device name: 'MX539730'INFO: Reading NK image to SDHC (please wait)...
INFO: Copying NK image to RAM address 0xa0200000
INFO: Read is 1% complete
INFO: Read is 2% complete
INFO: Read is 3% complete
INFO: Read is 4% complete
INFO: Read is 5% complete
INFO: Read is 6% complete
INFO: Read is 7% complete
INFO: Read is 8% complete
INFO: Read is 9% complete
INFO: Read is 10% complete
INFO: Read is 11% complete
INFO: Read is 12% complete
INFO: Read is 13% complete
INFO: Read is 14% complete
INFO: Read is 15% complete
INFO: Read is 16% complete
INFO: Read is 17% complete
INFO: Read is 18% complete
INFO: Read is 19% complete
INFO: Read is 20% complete
INFO: Read is 21% complete
INFO: Read is 22% complete
INFO: Read is 23% complete
INFO: Read is 24% complete
INFO: Read is 25% complete
INFO: Read is 26% complete
INFO: Read is 27% complete
INFO: Read is 28% complete
INFO: Read is 29% complete
INFO: Read is 30% complete
INFO: Read is 31% complete
INFO: Read is 32% complete
INFO: Read is 33% complete
INFO: Read is 34% complete
INFO: Read is 35% complete
INFO: Read is 36% complete
INFO: Read is 37% complete
INFO: Read is 38% complete
INFO: Read is 39% complete
INFO: Read is 40% complete
INFO: Read is 41% complete
INFO: Read is 42% complete
INFO: Read is 43% complete
INFO: Read is 44% complete
INFO: Read is 45% complete
INFO: Read is 46% complete
INFO: Read is 47% complete
INFO: Read is 48% complete
INFO: Read is 49% complete
INFO: Read is 50% complete
INFO: Read is 51% complete
INFO: Read is 52% complete
INFO: Read is 53% complete
INFO: Read is 54% complete
INFO: Read is 55% complete
INFO: Read is 56% complete
INFO: Read is 57% complete
INFO: Read is 58% complete
INFO: Read is 59% complete
INFO: Read is 60% complete
INFO: Read is 61% complete
INFO: Read is 62% complete
INFO: Read is 63% complete
INFO: Read is 64% complete
INFO: Read is 65% complete
INFO: Read is 66% complete
INFO: Read is 67% complete
INFO: Read is 68% complete
INFO: Read is 69% complete
INFO: Read is 70% complete
INFO: Read is 71% complete
INFO: Read is 72% complete
INFO: Read is 73% complete
INFO: Read is 74% complete
INFO: Read is 75% complete
INFO: Read is 76% complete
INFO: Read is 77% complete
INFO: Read is 78% complete
INFO: Read is 79% complete
INFO: Read is 80% complete
INFO: Read is 81% complete
INFO: Read is 82% complete
INFO: Read is 83% complete
INFO: Read is 84% complete
INFO: Read is 85% complete
INFO: Read is 86% complete
INFO: Read is 87% complete
INFO: Read is 88% complete
INFO: Read is 89% complete
INFO: Read is 90% complete
INFO: Read is 91% complete
INFO: Read is 92% complete
INFO: Read is 93% complete
INFO: Read is 94% complete
INFO: Read is 95% complete
INFO: Read is 96% complete
INFO: Read is 97% complete
INFO: Read is 98% complete
INFO: Read is 99% complete
INFO: Read is 100% complete
INFO: Copy of NK completed successfully
Either card is not eSD2.1, or boot partition is not created yet
Download successful! Jumping to image at 0x0 (physical 0x70200000)...
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0x8b
BSP Clock Configuration:
OSC = 24000000 Hz
PLL1 = 1000000000 Hz
PLL2 = 400000000 Hz
PLL3 = 400000000 Hz
PLL4 = 595000000 Hz
LP_APM = 24000000 Hz
ARM = 1000000000 Hz
AXI_A = 400000000 Hz
AXI_B = 200000000 Hz
EMI_SLOW = 133333333 Hz
AHB = 133333333 Hz
IPG = 66666666 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 400000000 Hz
ARM_AXI = 200000000 Hz
IPU_HSP = 200000000 Hz
VPU_AXI = 200000000 Hz
GPU = 200000000 Hz
GPU2D = 200000000 Hz
DEBUG_APB = 200000000 Hz
ENFC = 33333333 Hz
USBOH3 = 66666666 Hz
ESDHC1 = 100000000 Hz
ESDHC2 = 100000000 Hz
ESDHC3 = 100000000 Hz
ESDHC4 = 100000000 Hz
UART = 24000000 Hz
SSI1 = 6000000 Hz
SSI2 = 6000000 Hz
SSI3 = 6000000 Hz
SSI_EXT1 = 24000000 Hz
SSI_EXT2 = 19047619 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 297500000 Hz
DI0 = 50000000 Hz
DI1 = 297500000 Hz
VPU_RCLK = 24000000 Hz
SSI_LP_APM = 24000000 Hz
SPDIF_XTAL = 24000000 Hz
LDB_DIO = 595000000 Hz
LDB_DI1 = 595000000 Hz
SPDIF0 = 1142857 Hz
ESAI = 3000000 Hz
ESAI_HCKR = 0 Hz
ESAI_HCKT = 0 Hz
CAN = 66666666 Hz
FIRI = 24000000 Hz
CSI_MCLK1 = 25000000 Hz
CSI_MCLK2 = 25000000 Hz
ECSPI = 66666666 Hz
LPSR = 0 Hz
PGC = 8333333 Hz
ASRC = 59500000 Hz
IEEE_CEMX = 40000000 Hz
CKIH = 22579200 Hz
CKIH2 = 0 Hz
Windows CE Kernel for ARM (Thumb Enabled)
OEMInit: silicon ?= 0x21
BoardID = 0xc03.
Setting 1.2v regulator PLL1P2 to 1.3v
PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 WARNING: SRTC was reset.
PID:00400002 TID:011A006E UsbHost : New Function [address(1) / layer(0)]
PID:00400002 TID:00A20026 OTG : Load HCD
PID:00400002 TID:00A20026 OTG : Unload HCD
PID:00400002 TID:00A20026 OTG : Load UFN
PID:00400002 TID:00A20026 UfnClientLib!UfnCheckPID: WARNING -- using MS reference platform VID/PID 0x045e/0x00ce (not allowed in shipping platforms)
PID:00400002 TID:03640026 WARNING: possible performance issue: timeInit() not called, calling it in timeSetEvent()PID:00400002 TID:03640026 Pin muxing for Display pins complete.
PID:00400002 TID:03640026 KeybdDriverInitializeEx: Layout Manager successfully initialized to 1
PID:00400002 TID:03640026 LayoutMgrActivateKeyboardLayout: Called with hkl = 0x00000409
PID:01D70026 TID:05C00006 MSIM: IM_ReadRegistry read KB 5
PID:05C20006 TID:04980036 Explorer(V2.0) taskbar thread started.
PID:00400002 TID:03A20006 NDISPWR:: Found adapter [FEC1]