Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?

2,733 Views
sirrajrai
Contributor I

Hi,

I am new on the MCIMX6UL-EVK and Processor expert software.

I have to complete few task using processor expert software

1-make a hello world test project using arm cross compiler.

2-run this hello world remotely using linux on MCIMX6UL board.

I have completed first step but when i am trying to connect my board through SSH type connection the following error message is coming after entering user name and password-

Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed

My question is how many types of remote connection is possible to run my code.and also tell me that how i can i do SSH connection

before run my code i did the necessary required things like -

i have downloaded the fsl-image-gui-x11-imx6ulevk.sdcard linux image to SD card and set my board to SD card mode and then connect my board to ethernet cable.On terminal(Tera term) i have seen the Linux was booting but OpenSSH and Sftp was unable to install on that linux.

Thanks

Sirraj

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

2,364 Views
b36401
NXP Employee
NXP Employee

You need to install these services (ssh, etc) into the system you are running on the board.

For example you can add openssh-server package there.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,364 Views
sirrajrai
Contributor I

Hi Victor,

Thanks for ur reply

actually i had given these command on terminal to install openssh server(sudo apt-get install openssh-server) but it failed to install it.I faced error like

no  'sudo' command found 

no 'apt-get'  command found 

Due to this i am unable to install anything in rootfs.

i searched on net but didn't find necessary things so plz tell me how can i install openssh and update in

freescale linux.

I am currently using Xilinx SDK for MCIMX6UL board to load .elf file but finally i have to use processor expert so plz tell me how i can resolve error of apt-get and sudo.

Thanks

Sirraj

0 Kudos
Reply

2,364 Views
krishnakumar_ma
Contributor III

Is this problem resolved?. 

I too have a similar condition.

We have two NXP, S32v23 board. Step followed:

1. Boot the board with the default SD card.

2. Use eclipse to create a new remote connection to the board using SSH type. 

This result in error. 

Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException

I have tried connecting via putty and is able to get the prompt. 

How/What are the settings for the S32 studio to get the remote connection on the default boot-image of the board?.

0 Kudos
Reply