No sdcard image created

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No sdcard image created

Jump to solution
2,209 Views
cetzweiler
Contributor II

Build Configuration:
BB_VERSION        = "1.20.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-12.04"
TARGET_SYS        = "arm-poky-linux-gnueabi"
MACHINE           = "imx6dlsabresd"
DISTRO            = "poky"
DISTRO_VERSION    = "1.5.1"
TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU        = "vfp-neon"
meta             
meta-yocto        = "(nobranch):f1276b066223e7f501f7f711680215ff8edee252"
meta-oe           = "(nobranch):40e0f371f3eb1628655c484feac0cebf810737b4"
meta-fsl-arm      = "(nobranch):5fdb620c09df11e70434092f675c891e0ba84108"
meta-fsl-arm-extra = "(nobranch):251c07f9d868e0100ccf74fd1706269c8d6911fb"
meta-fsl-demos    = "(nobranch):5a12677ad000a926d23c444266722a778ea228a7"

Hello,

first timer here. I tried to "bitbake fsl-image-gui".

I get these errors:

ERROR: Function failed: do_rootfs (log file is located at /home/chuck/work/fsl-community-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.15734)
ERROR: Logfile of failure stored in: /home/chuck/work/fsl-community-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.15734ERROR: Task 7 (/home/chuck/work/fsl-community-bsp/sources/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'

When I look in build/tmp/deploy/images/imx6dlsabresd/ there is no .sdcard image there.

Can anyone help?

Thanks,

Chuck

Labels (3)
Tags (4)
1 Solution
1,992 Views
cetzweiler
Contributor II

Thank you for your time.

I'm sorry, I have little idea of what I'm doing.

I have a friend who tells me it may be something I put into the local.conf.

He told me to put back the original sample local.conf, do a -c clean and

see if it builds.

If it does, then it must be something I added to local.conf.

I'll contact you if this does not work.

Chuck Etzweiler | Integration Engineer

w. 814.235.1111 x394

e. [email protected]

<http://www.videon-central.com>

<https://plus.google.com/u/0/104238493788225182046/posts>

<http://www.linkedin.com/company/videon-central>

<https://www.facebook.com/videon.central>

On Fri, Mar 28, 2014 at 2:09 PM, Daiane Angolini <

View solution in original post

2 Replies
1,992 Views
daiane_angolini
NXP Employee
NXP Employee

This error says me nothing.

Could you, please share more lines of the error?

0 Kudos
Reply
1,993 Views
cetzweiler
Contributor II

Thank you for your time.

I'm sorry, I have little idea of what I'm doing.

I have a friend who tells me it may be something I put into the local.conf.

He told me to put back the original sample local.conf, do a -c clean and

see if it builds.

If it does, then it must be something I added to local.conf.

I'll contact you if this does not work.

Chuck Etzweiler | Integration Engineer

w. 814.235.1111 x394

e. [email protected]

<http://www.videon-central.com>

<https://plus.google.com/u/0/104238493788225182046/posts>

<http://www.linkedin.com/company/videon-central>

<https://www.facebook.com/videon.central>

On Fri, Mar 28, 2014 at 2:09 PM, Daiane Angolini <