No MIPI DSI clock available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No MIPI DSI clock available

1,701件の閲覧回数
senizhuseyin
Contributor I

Hello,

I am trying to run a MIPI DSI display on savageboard-quad of which processor is imx6q. I am using the Yocto release provided by saveboard site. Kernel Version is 3.0.35. I have enabled MIPI DSI host controller driver and Himax HX8369A MIPI DSI panel in Kernel configuration. I am using Himax HX8394F MIPI DSI panel. So I ported current  HX8369A code for HX8394F.

I can see that the driver is probed and initialized in the kernel logs. But LCD_ID is not read at all. I got 0x00 for LCD_ID. I analyzed the signals with scope. Data lane signals seem to have expected waveforms. But MIPI DSI clock signals are not as I would expect. Both have 1V DC for a long time, than it toggles, and goes back to 0V and stay still.

What can be the reason beyond No MIPI DSI clock issue? I tried to trace video_27m_clk_root in the kernel, but no clue at all.

Regards,

Seniz

ラベル(4)
0 件の賞賛
返信
0 返答(返信)