Nitrogen6x Gstreamer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,280件の閲覧回数
rashmib
Contributor I

Hi,

Can anybody tell me , from where I can get the gstreamer source code to test on imx6 nitrogen6x board and which version of gstreamer should be used .

Thanks,

Rashmi

ラベル(3)
0 件の賞賛
返信
1 解決策
2,215件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rashmi

seems one can look at

https://boundarydevices.com/gstreamer-imx-plugin-with-buildroot/ 

GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms 

or search https://boundarydevices.com/?s=Gstreamer 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,216件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rashmi

seems one can look at

https://boundarydevices.com/gstreamer-imx-plugin-with-buildroot/ 

GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms 

or search https://boundarydevices.com/?s=Gstreamer 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,215件の閲覧回数
rashmib
Contributor I

Hi igor,

Thanks for the reply.

Now I am able to use  gstreamer with  the build root image from the above link which you mentioned.

Now I want to test my own gstreamer application. Can you please let me know where I can get the toolchain which is used for the build root image.

Thanks,

Rashmi

0 件の賞賛
返信