Need support for PCm5242 Bringup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need support for PCm5242 Bringup

5,792件の閲覧回数
divyeshmarne0
Contributor III

Hi Team,

We are working on PCM5242 Audio DAC with NXP processor in ANdorid11 code base.

I have integrated all the changes in DTSI and driver file.

After changes, DAC has been registered successfully. 

I checked the all clocks like WCLK MCLK BCLK and DIN pin , We are getting all the clocks properly while playing audio file. But NO sound.

Error we are facing:

E audio_hw_primary: start_output_stream: Invalid PCM card id: -1
I audio_hw_primary: start_output_stream: primary: 1, out: 0xee944630, device: 131072, address: , mode: 0, flags 0x2
I audio_hw_primary: select_output_device(), headphone 0 ,headset 0 ,speaker 2
D audio_hw_primary: start_output_stream: pcm_open: card: -1, pcm_device_id: 0, rate: 48000, channel: 2, format: 0, period_size: 0xc0, flag: 9

 

Looks like no card present:

evk_8mm:/ # cat /proc/asound/card0/pcm0p/*
card: 0
device: 0
subdevice: 0
stream: PLAYBACK
id: 30050000.sai-pcm512x-hifi pcm512x-hifi-0
name: 30050000.sai-pcm512x-hifi pcm512x-hifi-0
subname: subdevice #0
class: 0
subclass: 0
subdevices_count: 1
subdevices_avail: 1

I2C dump:

1. When audio not playing:

 

divyeshmarne0_6-1663662938852.png

 

 

2. When trying to play audio file

 

divyeshmarne0_5-1663662922815.png

 

 

DTSI changes:

sound-pcm512x {
compatible = "simple-audio-card";
simple-audio-card,name = "pcm512x-audio";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&dailink0_master4>;
simple-audio-card,frame-master = <&dailink0_master4>;

simple-audio-card,widgets =
"Line", "Left Line Out Jack",
"Line", "Right Line Out Jack";
simple-audio-card,routing =
"Left Line Out Jack", "OUTL",
"Right Line Out Jack", "OUTR";
dailink0_master4: simple-audio-card,cpu {
sound-dai = <&sai5>;
};
simple-audio-card,codec {
sound-dai = <&pcm5242>;
clocks = <&clk IMX8MM_CLK_SAI5_ROOT>;
};
};

 

pcm5242: pcm5242@4c {
compatible = "ti,pcm5242";
#sound-dai-cells = <0>;
reg = <0x4c>;
AVDD-supply = <&reg_3v3_vext>;
DVDD-supply = <&reg_3v3_vext>;
CPVDD-supply = <&reg_3v3_vext>;
clocks = <&ext_osc_22m>, <&ext_osc_24m>;
clock-names = "sclk0", "sclk1";
};

&sai5 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai5>;
assigned-clocks = <&clk IMX8MM_CLK_SAI5>;
assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
assigned-clock-rates = <24576000>;
status = "okay";
};

pinctrl_sai5: sai5grp {
fsl,pins = <
MX8MM_IOMUXC_SAI5_MCLK_SAI5_MCLK 0xd6 /*MCLK*/
MX8MM_IOMUXC_SAI5_RXD2_SAI5_TX_BCLK 0xd6 /*BCLK*/
MX8MM_IOMUXC_SAI5_RXD3_SAI5_TX_DATA0 0xd6 /*DIN*/
MX8MM_IOMUXC_SAI5_RXD1_SAI5_TX_SYNC 0xd6 /*WCLK*/
>;
};

 

NOTE: WE dont have proper driver. We are using driver of different family which is pcm5142.

sound/soc/codecs/pcm512x-i2c.c

sound/soc/codecs/pcm512x.c

Need your urgent support

Thanks

Divyesh

 

0 件の賞賛
返信
7 返答(返信)

5,783件の閲覧回数
qwerty1
Contributor I

Hi @divyeshmarne0 

Android layer changes are required related to "PCM5242 Audio DAC"

0 件の賞賛
返信

5,779件の閲覧回数
divyeshmarne0
Contributor III

Hi @qwerty1 ,

Could you please specify the what changes required?

Please share any reference.

 

Thanks

Divyesh

0 件の賞賛
返信

5,777件の閲覧回数
qwerty1
Contributor I

Sorry, I don't have any reference.

First check in device/nxp folder [Files- audio_policy_configuartion and audio_effects.xml]. Then vendor folder[Audio HAL changes]

0 件の賞賛
返信

5,776件の閲覧回数
qwerty1
Contributor I
as per log its identifying your card id as -1. You need to update this in Audio HAL changes
0 件の賞賛
返信

5,773件の閲覧回数
divyeshmarne0
Contributor III
means exactly what need to be done?
0 件の賞賛
返信

5,789件の閲覧回数
divyeshmarne0
Contributor III

Please find below logs:

01-01 00:00:00.234 0 0 E imx-pcm512x sound-pcm512x: failed to find codec device
01-01 00:00:01.148 0 0 E pcm512x 3-004c: divyesh enter into CONFIG_OF func :pcm512x_probe
01-01 00:00:01.155 0 0 E pcm512x 3-004c: divyesh enter into CONFIG_OF and dev->of_node func :pcm512x_probe

divyeshmarne0_0-1663668245637.png

 

0 件の賞賛
返信

5,768件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

FYI. Please read the Chapter 16 for audio codec porting.

https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf

 

0 件の賞賛
返信