Need board to connect RPI-CAM-MIPI to iMX8M-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need board to connect RPI-CAM-MIPI to iMX8M-EVK

6,324件の閲覧回数
roberthougen
Contributor I

I have a i.MX8M-EVK and want to connect a RPI-CAM-MIPI to it.
The picture on your web site shows two boards included in the RPI-CAM-MIPI, but when I received it there was only one board.
The 22pin FFC to mini-SAS adaptor board was not included. The picture shows the board part number as 700-55271 REV X3.
Is there a way I could buy this board, or could NXP provide the design files including schematic and board layout so I can have one made?

Thank you

0 件の賞賛
返信
5 返答(返信)

5,971件の閲覧回数
SHager
Contributor I

I can undestand Roberts Question well. I am also interested in the board RPI-CAM-MINISAS which should be included in the Product RPi-CAM-MIPI according to the documentation (See Board Kit Contents in https://docs.nxp.com/bundle/UM11933/page/topics/rpi-cam-mipi_overview.html).

Thank you Brian for giving the link to the design files.

Unfortunately the RPI-CAM-MINISAS is not part of this files in PDF Format. Are there any additional Schematics for that board?

0 件の賞賛
返信

6,265件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @roberthougen,

Yes, you can download the design files for this product at the following link:

Link to download RPI-CAM-MIPI design files 

Have a great day!

Best regards, Brian!

0 件の賞賛
返信

5,820件の閲覧回数
vihang_vinayak
Contributor II

Hi Brian,

Can you please provide the design files for the RPI-CAM-MIPI board with MiniSAS connector i.e the 700-55271 design files.

vihang_vinayak_1-1706704517931.png

 

We are using the i.MX8X-EVK development board with MiniSAS connector for camera interface where the above RPI-CAM-MIPI board with MiniSAS connector i.e the 700-55271 design can help us to integrate different camera modules with i.MX8M-EVKit

Regards,

Vihang Waze

 

5,933件の閲覧回数
Ryo_Aoki
Contributor III

>The picture on your web site shows two boards included in the RPI-CAM-MIPI, but when I received it there was only one board.
>The 22pin FFC to mini-SAS adaptor board was not included. 

 

I also purchased RPI-CAM-MIPI, but the mini-SAS adapter board was not included.

Does this mean that this board is not included in RPI-CAM-MIPI?

4,338件の閲覧回数
robinb
Contributor I
Indeed. I purchased the set with the camera pictured with the adapter and it was also listed by the distributor. I was shocked and frustrated when it was not in the box. It looks like NXP has stopped making them.

In the end I started developing the driver on a raspberry pi instead but it's far from ideal.

There has been a picture of a board with 4 mini-sas connectors to one 22pin FPC connector floating around in NXPs applicationnotes/starting guides but I can't find that product.

Technexxion makes modules as well but they all have an ISP on them that can not be bypassed without heavy modifications.
0 件の賞賛
返信