NVCC_LVDS_2P5 current consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVCC_LVDS_2P5 current consumption

ソリューションへジャンプ
3,132件の閲覧回数
gavinjones
Contributor I

Dear Community,

In my iMX6Q application I am not using the LVDS interface. However, the datasheet states that the NVCC_LVDS_2P5 supply must be provided, as it also powers the DDR I/O pre-drivers. What is the maximum current consumption from this supply when LVDS is not used (the DDR will be used extensively)?


Thanks,

Gavin.


ラベル(3)
0 件の賞賛
返信
1 解決策
2,911件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Gavin

     I think you can just use the max VDDHIGH_IN power consumption to be the number you want, although it includes the PLL's power consumption. So ideally this VDDHIGH_IN's power consumption is higher than the actually max power of NVCC_LVDS_2P5. The typical max power of VDDHIGH_IN is around 85mA, so this 85mA exceed your platform's 2p5 power rail's capability? If you really want to get the real max power of NVCC_LVDS_2P5, then you may need to measure the power consumption on our SabreSD board, remove r600 and connect a current meter, then run the max power test case.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,911件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gavin,

You can calculate power measurements using the following application note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

Let me know if you have any questions.

0 件の賞賛
返信
2,911件の閲覧回数
gavinjones
Contributor I

Hello SerchMX,

AN4509 gives me a typical value for the current consumption into the VDDHIGH_IN pin. However, it does not break this figure down between the direct internal loads (PLLs) and the loads externally connected to the VDDHIGH_CAP pin (including NVCC_LVDS_2P5). Maximum values for a number of the loads are given in the data sheet, section 4.1.5, but NVCC_LVDS_2P5 is not included.

My application already has a 2.5V switching regulator supplying some of the iMX6 IOs. Therefore, for improved power efficiency, I plan to connect all the iMX6 2V5 loads (including NVCC_LVDS_2P5) directly to this rail, rather than to the VDDHIGH_CAP pin. However, I need to know the maximum current consumption of the NVCC_LVDS_2P5 load so as to ensure the switching regulator is rated high enough.

Please can you provide an upper bound for the maximum current consumption of the NVCC_LVDS_2P5 load?

Best regards,

Gavin.

0 件の賞賛
返信
2,912件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Gavin

     I think you can just use the max VDDHIGH_IN power consumption to be the number you want, although it includes the PLL's power consumption. So ideally this VDDHIGH_IN's power consumption is higher than the actually max power of NVCC_LVDS_2P5. The typical max power of VDDHIGH_IN is around 85mA, so this 85mA exceed your platform's 2p5 power rail's capability? If you really want to get the real max power of NVCC_LVDS_2P5, then you may need to measure the power consumption on our SabreSD board, remove r600 and connect a current meter, then run the max power test case.

0 件の賞賛
返信
2,911件の閲覧回数
gavinjones
Contributor I

Hi Yongcai,

Thanks for the response. I was hoping for a lower figure, but I can budget for the full 85mA for now. I will make the measurement when we get the board busy.

Best regards,

Gavin.

0 件の賞賛
返信