NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

1,708 Views
SumitVaidya
Contributor II

Hi,

 

Recently I was able to boot IMX6 evaluation board successfully with linux as my OS.

I was browsing through the uboot source code for checking partition for uboot, linux kernel and rootfs on the NOR flash. I downloaded source code for bootloader using 'ltib' command.

 

As per my understanding, NOR flash should be divided into 3 partitions as uboot, kernel and rootfs.

Is there a way to find this partition table along with their load address in linux kernel source code? Also if there is any command to download linux kernel source code using LTIB?

 

Thanks in advance.

 

Regards,

Sumit

Tags (1)
0 Kudos
Reply
0 Replies