NAND Flash on iMX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NAND Flash on iMX53

2,509 次查看
jomeke
Contributor II

Hi guys,

is there anybody who has a desin example from a NAND flash connected to the iMX537 ?

标签 (1)
0 项奖励
回复
3 回复数

2,136 次查看
jomeke
Contributor II

Thanks for the information Florent

Florent Auger said:

Hi

 

The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.

You'll find there that the NAND control signals are dedicated pins with the same name.

Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.

 

At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.

 

You can check that board for a reference:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIM...

0 项奖励
回复

2,136 次查看
FlorentAuger
Contributor V

Hi

 

The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.

You'll find there that the NAND control signals are dedicated pins with the same name.

Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.

 

At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.

 

You can check that board for a reference:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABREAUTO&fpsp=1&tab=Design_To...

0 项奖励
回复

2,136 次查看
hoanghoa
Contributor I

Hi guys,

I am porting u-boot for an mx53 board which has 512 MB Nand flash of Samsung K9F4G08.

It uses CS0 and 8 bit interface only. So which value should be for CONFIG_SYS_NAND_BASE?

The connection signal is below:

- NANDF_CS0  --> CS (to NAND chip)

- NANDF_CS1,2,3 --> not used

- PATA_DATA[0-7] --> DATA[0-7]

Expecting your help!!

HTH

0 项奖励
回复