Mouse problem on i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mouse problem on i.mx6

1,512 Views
浩卢
Contributor III

Hi

I run linux+qt on i.mx6q.The mouse in the use of the process, suddenly can not be used, the serial port does not print any error messages, after re plug  the mouse still can not be used, but the keyboard can be used.

someone hlep me please,Thanks.

Labels (3)
0 Kudos
Reply
2 Replies

1,382 Views
art
NXP Employee
NXP Employee

Yes, the similar problem is observed sometimes when using a low-speed USB devices such as mices and keyboards. Try to connect your mouse and keyboard through an external USB Hub.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,382 Views
浩卢
Contributor III

Hi Artur Petukhov 员工

  Thanks for your reply.I will  try for it.

0 Kudos
Reply