Mounting Samba Shares

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mounting Samba Shares

1,380 Views
DejanDeletic
Contributor I

I'm running the Ubuntu from the SD card delivered with the i.MX53 QSB (i.e. Lucid, kernel version 2.6.35.3-1129-g691c08a). 

I cannot mount samba shares from command line. No problem accessing same shares from nautilus (file manager). 

ddd@iMX53:~$ sudo mount.cifs //192.168.0.1/P_Drive /mnt/netdrv/
[sudo] password for ddd:
Password:
mount error: cifs filesystem not supported by the system
mount error(19): No such device
Refer to the mount.cifs(8) manual page (e.g. man mount.cifs)

It appears cifs kernel module is missing

ddd@iMX53:~$ sudo modprobe fuse
FATAL: Module fuse not found.

ddd@iMX53:~$ ll /lib/modules/`uname -r`/kernel/fs
total 8.0K
drwxr-xr-x 2 root root 4.0K 2011-10-07 05:21 autofs4/
drwxr-xr-x 2 root root 4.0K 2011-10-07 05:21 nls/

Has anyone come across this issue? I'd expect to see cifs.ko in '.../kernel/fs' directory. How can I add this module? 

Thanks,

Dejan

Tags (2)
0 Kudos
Reply
0 Replies